Technical FAQs

Ask a Question

What communication cables are required to communicate between the HMISTU655/855 and a Mitsubishi FX1 PLC?

 Title

What communication cables are required to communicate between the HMISTU655/855 and a Mitsubishi FX1 PLC? 

Issue

 

Product Line

HMISTU655; HMISTU855; Mitsubishi FX1 

Environment

 

Cause

Resolution

The communications cable between the HMISTU655/855 to the Mitsubishi FX PLC is the  XBTZ980 cable  and the XBTZG939 adapter.

Was this helpful?
What can we do to improve the information ?