Technical FAQs

Ask a Question

How do you enable user defined shutdown values for the outputs of the 170ANR12091 Momentum I/O module?

Title

Enable user defined shutdown values for the 170ANR12091 I/O module

Issue

 

Product Line

Modicon Momentum

Environment

 

Cause

 

Resolution

In order to enable the user defined shutdown values of this module, the following has to be done:
In output word 1 of the module, Bit 15 has to be set to a 1 to enable the user defined shutdown values.
 

Was this helpful?
What can we do to improve the information ?