Technical FAQs

Ask a Question

Can the Modbus port on the terminals of the 170ADM54080 be used to program the Momentum CPU?

Title

170ADM54080 Modbus port programming

Issue

 

Product Line

Modicon Momentum

Environment

 

Cause

 

Resolution

No, this port is a Modbus Master RS485 port designed to communicate to MCC (motor control center) devices which only have a small amount of data available.

Was this helpful?
What can we do to improve the information ?