Technical FAQs

Ask a Question

What is the transmission speed of data on a Momentum IObus network?

Title

Momentum IO bus network speed

Issue

 

Product Line

Modicon Momentum

Environment

IO Bus network

Cause

 

Resolution

Data is transmitted at 500 kbits/s on an IObus network.

Was this helpful?
What can we do to improve the information ?