Technical FAQs

Ask a Question

What is the maximum Ethernet cable length between Lexium Integrated Drives?

The Lexium Integrated Drive type ILx2K have an internal "EthernetIP switch".
Therefore a maximum cable length of 100m is allowed between each daisy chained "EthernetIP slave" such as the ILA2K.
This is according the specification of the ODVA.
Was this helpful?
What can we do to improve the information ?