Technical FAQs

Ask a Question

Momentum High Speed counter (170AEC92000) sample application using the AEC DFB to show a configuration for an Upcounter (Mode 2) with modulo and outputs

Title

AEC DFB example for Mode 2 with module value and outputs configured.

Issue

 

Product Line

Modicon Momentum

Environment

 

Cause

Resolution

See attached pdf file

Was this helpful?
What can we do to improve the information ?