Technical FAQs

Ask a Question

Momentum High Speed counter (170AEC92000) sample application using the AEC DFB to show a configuration for a Pulse counter with external time base (Mode 8).

Title

AEC DFB example for Mode 8

Issue

 

Product Line

Modicon Momentum

Environment

 

Cause

 

Resolution

See attached pdf file

Was this helpful?
What can we do to improve the information ?