Technical FAQs

Ask a Question

Do the Advantys STB Reflex actions work without having a Field bus connected or communicating ?


Advantys STB reflex actions



Product Line

Advantys STB






Yes, the Reflex actions will work without communications to a Field bus, when the following conditions are true:

  • Two channel output modules with both channels configured for reflex actions.
  • Neither of these reflex actions is receiving any inputs from the NIM (inputs to the reflex blocks are not coming from the virtual module/master PLC or from the action module itself).

Note: Only two-channel output modules are supported.

Was this helpful?
What can we do to improve the information ?