Technical FAQs

Ask a Question

How do you change the default username and password on the Advantys STB Ethernet NIM STBNIP2212 ?

Title

STBNIP2212 web pages username and password

Issue

 

Product Line

Advantys STB

Environment

 

Cause

 

Resolution
Once you are connected to the web pages via the default username "USER" and password of "USER", follow this procedure:

1.  Click on the Security tab.
2.  Select the Change Web Access Password option.
3.  Type the new user name. (The user name can have a maximum of eight alphanumeric characters. You can also use an underscore (_). The characters are case-sensitive.)
4.  Type the user name again to Confirm New User Name field.
5.  In the New Password field, type your web access password. (The password can have a maximum of eight alphanumeric characters. You can also use an underscore (_). The characters are case-sensitive.)
6.  Type the password again in the Confirm New Password field.
7.  Click on the Save button.

The web access user name and password will take effect immediately.
 

 

 

Was this helpful?
What can we do to improve the information ?