Technical FAQs

Ask a Question

What is the maximum number of counts available from the multiturn encoder for Lexium Integrated Drives?

The optional multiturn absolute encoder for Lexium ILA and ILS drives has the following maximum counts.
16384 counts x 4096 turns - 1 = total maximum counts of 67108863

Was this helpful?
What can we do to improve the information ?