Technical FAQs

Ask a Question

Is there a Momentum IO base which handles 12VDC applications?

Title

Momentum I/O bases which support 12vdc

Issue

 

Product Line

Modicon Momentum

Environment

12vdc

Cause

 

Resolution

Yes, there are two modules, the 170ADM85010 and the 170AMM09001. The 170ADM85010 is a 10 to 60 VDC IO base, which has 16 discrete inputs and 16 discrete outputs available. The 170AMM09001 is a mixed IO base, which has 4 analog inputs, 2 analog outputs, 4 discrete inputs and 2 discrete outputs.

Was this helpful?
What can we do to improve the information ?