Technical FAQs

Ask a Question

Does Schneider Electric offer the Berger Lahr RDM36/12 2 phase stepping motor with ID number 13981350026

No,  the RDM36/12 with ID number 13981350026 is a special version of RDM36/12 with a 62.5:1 gearbox integrated to the motor.
This is offered only to the OEM due to the unique 62.5 : 1 gearbox. 
 
You must contact the OEM machine manufacturer for which the motor was incorporated to see if they can provide this motor type as a spare.
Was this helpful?
What can we do to improve the information ?