Technical FAQs

Ask a Question

What causes error "Reduce number of cards set in traffic cop" in ProWorx Nxt?

This error is displayed when not enough IO words are configured to accommodate the number of IO cards being configured.
Go to <Configuration><<General> and increase the number of I/O Words.
Was this helpful?
What can we do to improve the information ?