Technical FAQs

Ask a Question

Does the Lexium 05 support BMH motors?

No, BMH motors are not compatible with Lexium 05 drives due to the type of encoder that is used in these motors.
If a BMH motor is connected to a Lexium 05, the drive will display fault 7120 which indicates that invalid motor data has been read. 
Was this helpful?
What can we do to improve the information ?