Technical FAQs

Ask a Question

Unable to create an unbuffered report control block for a MiCOM 40 series relay

Issue: Unable to assign a dataset to a unbuffered report control block

Product Line: MiCOM 40 series

Resolution: In order to assign a dataset to a report control block, the dataset must be in the same logical node as the report control block. By default the report control blocks are located in the system logical node. When creating the dataset ensure that the LLNO it is assigned to is the system node. Once the dataset is in the system node the dataset will be visible to the report control block.

Keywords: MiCOM dataset, Logical Node, LLNO, Report control block
Was this helpful?
What can we do to improve the information ?