Technical FAQs

Ask a Question

What is the part number for the jumper used on the Quantum field wiring terminal strip?

Title

What is the part number for the jumper used on the Quantum field wiring terminal strip?

Issue

 

Product Line

Modicon Quantum

Environment

 

Cause

 

Resolution

The part number is 140XCP60000, this package includes 12 jumpers. The jumper is a two-position jumper.

Was this helpful?
What can we do to improve the information ?