Technical FAQs

Ask a Question

What web browsers are supported for viewing COM'X 200 web pages?

Issue:
Some web browsers are not supported to view COM'X 200 web pages

Product Line
COM'X 200

Environment
Google Chrome
Internet Explorer 8
Firefox 15
Opera 11.6
Safari 5.1

Cause
COM'X 200 web pages cannot be viewed in an unsupported browser

Resolution
Officially the COM'X 200 supports the following web browsers:

Chrome24
Internet Explorer 8
Firefox 15
Opera 11.6
Safari 5.1

The COM'X 200 has been tested successfully to work on Internet Explorer 9 and Internet Explorer 10 although they are not officially supported.
Was this helpful?
What can we do to improve the information ?