Technical FAQs

Ask a Question

G3200 error message RptEnabled 'bad max' attribute value (2) or too much reports (2 > 0)

Issue: When attempting to create a CID file for a modbus device using he G3200 I receive an error which is displayed in the G3200 Summary located in the Diagnostics section of the G3200 webpage.

Product Line: G3200

Resolution: The RptEnabled 'bad max' attribute value (2) or too much reports (2 > 0) is due to a lack of the service for the IED. To resolve this error the service capability must be added to the IED. Locate the Services section for the IED (not the logical device) and add the following line:
<ConfReportControl max="16"/>
The maximum number will vary according to your needs. The order in which this service is added does not affect functionality it simply must be in the services section

Keywords: G3200, RptEnabled, bad max attribute
Was this helpful?
What can we do to improve the information ?