Technical FAQs

Ask a Question

Was is the pin assignment of the CN3 connection for the RS485 port on Lexium 23?

Lexium 23 supports RS485 communication via the CN3 connection on the front of the drive.
Pin assignment of the RS485 is as follows.
Pin 4 = RS485+
pin 5 = RS485-

See attachment for greater details.


Was this helpful?
What can we do to improve the information ?