Technical FAQs

Ask a Question

ION Setup 3.0 Error after Installation

Issue:
Upon closing ION Setup for the first time after it has been installed the user may receive the following error.

Program Compatibility Assistant

This program might not have installed correctly





Product Line:
ION Setup 3.0

Environment:
Software Installation

Cause:
The Windows user account that performed the installation may not have write access to the registry and Program Files (x86) directory.

Resolution:
Ensure the you are logged into Windows with a user that has the required permissions to write to the registry and Program Files (x86) directory.

 
Was this helpful?
What can we do to improve the information ?