Technical FAQs

Ask a Question

What safety category is the STO function of the Lexium SD32x stepping motor drive?

The STO function is also known as "Power Removal" which as the name implies disables the power stage and removes power from the motor causing the motor to lose all torque.
The STO function by itself  is category 0 but can be raised to category 1 with the additional of an approved E-Stop module.
Was this helpful?
What can we do to improve the information ?