Technical FAQs

Ask a Question

Does Lexium SD32x stepper controller support Profibus communication?

Title:
 

Does Lexium SD32x stepper controller support Profibus communication?
 

Issue:

Customer wants to control his stepper motor from a Siemen's PLC over Profibus.
 

Product Line:

Motion - Lexium SD32x

Environment:

 

Profibus

Cause:

Replacing a Twinline Stepper Controller using Profibus communication to the current platform.

Resolution:

Yes, the Stepper controller bearing part number SD328BU68S2 supports (B = Profibus) Profibus communications and hence can be used on a Profibus network.
Was this helpful?
What can we do to improve the information ?