Technical FAQs

Ask a Question

Unable to add MMXU parameters to existing dataset for Sepam in CET850 software.

Issue:
When modifying an existing dataset for a Sepam relay, no additional MMXU parameters are available.

Product Line:
Sepam

Cause:
Functional Contraint limitations

Resolution:
Please use the attached document for details. To resolve the issue the functional constraint parameter must be changes to MX.

 

Was this helpful?
What can we do to improve the information ?