Technical FAQs

Ask a Question

Why does the variable report & function do not work in Vijeo Designer v6.1 SP4?


 

Title

Why does the variable report & function do not work in Vijeo Designer v6.1 SP4?

Issue

xxxxxxx
 

Product Line

Vijeo Designer
 

Environment

xxxxxxx
 

Cause

xxxxxxx
 

Resolution

The variable report & function does not work in Vijeo Designer v6.1 SP4. This is a known issue and will be resolved in the upcoming release of Vijeo Designe v6.2. The only way to produce a variable report is to use the "Report All" function. However, you cannot access the cross reference variables.
 

Was this helpful?
What can we do to improve the information ?