Technical FAQs

Ask a Question

Where are the MFB eds files for Lexium05, Lexium15, Lexium17 and Lexium 32, used with Unity Pro and Sycon software located?

Title
Location of  the Motion Function block (MFB) eds files for Lexium05, Lexium15, Lexium17 and Lexium 32, used with Unity Pro and Sycon software
 
Issue
When using a Unity Premium processor with a TSXCPP110 CANopen PCMCIA card and Sycon software, the motion function block (MFB) eds files have to be added to the the Sycon software. The files will have to be copied to the directory located at C:\Program Files\Schneider Electric\SyCon\Fielbus\CANopen\EDS
 
Product Line
Lexium05, Lexium15, Lexium17, Lexium 32
 
Environment
Unity Pro v7.0, Sycon v2.9
 
Cause
The MFB eds files for Lexium05, Lexium15, Lexium17 and Lexium 32 are not part of the original Sycon software catalog,
 
Resolution
The MFB eds files for Lexium05, Lexium15, Lexium17 and Lexium 32, used with Unity Pro and Sycon software are located in the following folder:
Windows XP: C:\Documents and Settigs\All Users\Application Data\Schneider Electric\ConfCatalog\Database\Motion\EDS.
Windows 7: C:\ProgramData\Schneider Electric\ConfCatalog\Database\Motion\EDS
In order to be able to add these files to the Sycon configuration and then to Unity Pro, the required MFB eds files will have to be copied to the directory located at C:\Program Files\Schneider Electric\SyCon\Fielbus\CANopen\EDS

 
Was this helpful?
What can we do to improve the information ?