Technical FAQs

Ask a Question

Can you setup customized bitmaps for the status of the push button switch in Vijeo Designer?

Issue:
Can you setup customized bitmaps for the status of the push button switch in Vijeo Designer?

Product Line:
Vijeo Designer

Resolution:
Yes, you can setup customized bitmaps for the status of the switch.  You need to change the category to "User Defined" from the General tab of the switch settings.  Then in the Color tab, select the "Browse" button from the [Up] and [Down] to select your bitmap image.

 

Was this helpful?
What can we do to improve the information ?