Technical FAQs

Ask a Question

What size gauge conductors (AWG or mm^2) does the TCSXCNDMNX3V cable have?

Title

Wire gauge size of the TCSXCNDMNX3V cable

Issue

 

Product Line

TM7 I/O

Environment

 

Cause

 

Resolution

The conductor cross section is 0.34 mm^2 or (AWG 22).

Was this helpful?
What can we do to improve the information ?