Technical FAQs

Ask a Question

Are the motor cables and encoder cables for Lexium SD3 stepper drives approved for cable tray installation?

Yes, the manual for Lexium SD3 indicates that the motor and encoder cable for Lexium SD3 are approved for drag chain applications.
The manual also provides minimum bend radius for fixed and moving installations.
Was this helpful?
What can we do to improve the information ?