Technical FAQs

Ask a Question

What motor cables are offered for use with BRS stepping motors that have connectors?

The prefabricated cables for use with BRS stepping motors are as follows.

Motor cable for stepper motor 4 x 1.5 shielded, motor end with 6-pin circular connector; other cable end open; length 3 m = VW3S5101R30
Motor cable for stepper motor 4 x 1.5 shielded, motor end with 6-pin circular connector; other cable end open; length 5 m = VW3S5101R50
Motor cable for stepper motor 4 x 1.5 shielded, motor end with 6-pin circular connector; other cable end open; length 10 m = VW3S5101R100
Motor cable for stepper motor 4 x 1.5 shielded, motor end with 6-pin circular connector; other cable end open; length 15 m  = VW3S5101R150
Motor cable for stepper motor 4 x 1.5 shielded, motor end with 6-pin circular connector; other cable end open; length 20 m  = VW3S5101R200
Was this helpful?
What can we do to improve the information ?