Technical FAQs

Ask a Question

Is there a way to search for variable/variable types in Unity Pro?

Title
Is there a way to search for variable/variable types in Unity Pro?

Issue
Trying to search for variable in Unity Pro.

Product Line
Unity Pro

Resolution
To search in Unity go to the toolbar at the top of the screen and select Tools --> Search/Replace.



Once Search/Replace is selected, a Cross-References window will appear. In that window select the Show / hide search dialog button



The Data Search window will pop up. From there you can search in the Find What field or Browse using the button to the right of the Find What field.



If browsing is preferred, select the Browse button and the Cross-References : Data Selection will appear, where you can go through the Variable, Variable Types, Function Blocks, and Function and Function Block Type tabs to search for any entity inside the Unity project. 



 
Was this helpful?
What can we do to improve the information ?