Technical FAQs

Ask a Question

Can Vijeo Designer v6.2 open projects with previous versions?

Vijeo Designer v6.2 can open applications that are created with the following versions:

  • Vijeo Designer v5.1 (and associated patches)
  • Vijeo Designer v6.0 (and associated patches)
  • Vijeo Designer v6.1 (and associated patches)
If the project is older than v5.1, then open the project is v6.1, export it back out to a VDZ, and then import into v6.2. 
Was this helpful?
What can we do to improve the information ?