Technical FAQs

Ask a Question

Is Vijeo Designer Web Gate compatible with Internet Explorer 64 bit?

Title

Is Vijeo Designer Web Gate compatible with Internet Explorer 64 bit? 

Issue

 

Product Line

Vijeo Designer, Magelis XBTGC/GK/GT, HMIGTO/STO/STU

Environment

 

Cause

Resolution

No, as of Vijeo Designer v6.2 SP2.1, Web Gate is not compatible with Internet Explorer 64 bit.  It will only work on the 32 bit version.

Was this helpful?
What can we do to improve the information ?