Technical FAQs

Ask a Question

How do I disable/enable communications to an Equipment from Vijeo Designer?


 Can I disable/enable communications to a driver equipment from Vijeo Designer?


 This knowledge article is to show customer's how to disable/enable communications to an Equipment.

Product Line

 Vijeo Designer





You can use the system control words to access information or perform operations on the driver.  Below are the instructions to create a variable to
disable/enable the driver and equipment:
1 - Create a new variable
2 - In the New Variable dialog box, set Data Type as INT, Data Source to External, and select the Scan Group of the equipment driver.
3 - In the Device Address field, type @sys:1

@sys:1 controls the state of the communications.

You can write the values 1 or 0 to turn on (1) or off (0) the communication with the associated equipment.  A value of 2 indicates the driver is offline for this specific equipment.

Was this helpful?
What can we do to improve the information ?