Technical FAQs

Ask a Question

How do I wire a 2-wire transmitter to an Advantys STB analog current input module?

The following wiring diagram indicates how to wire a 2-wire transmitter to the STBACI1230 or the STBACI1225 analog current input module.Loop supply voltage is provided by the PDM.


      Pin 1 +24VDC for sensor
      Pin 2 input from sensor
      Pin 4 return from input
      Pin 6 +24VDC return
Was this helpful?
What can we do to improve the information ?