Technical FAQs

Ask a Question

What are the states of the relay outputs of an Advantys STBDRC module when a loss of Field Bus communication, PDM power, or NIM power occurs?

When a loss of the field bus communication occurs, the relay outputs will go to their configured fallback states. When a loss of PDM or NIM power occurs, the internal relays become de-energized causing the outputs to go to their de-energized state regardless of the configured fallback state. For example a normally open output(contact) will go to zero(open) and a normally closed output(contact) will go to one(close).
Was this helpful?
What can we do to improve the information ?