Technical FAQs

Ask a Question

Why can I only link one of my two M340 NOE modules to the Ethernet network that I created?

Each module requires it's own Ethernet Network configuration. Once a network is linked, it can no longer be linked to a different module. Create a second network and link it to the second NOE module.


Legacy KB System (APS) Data: RESL213338 V1.0, Originally authored by DaSo on 01/29/2014, Last Edited by DaSo on 01/29/2014
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?