Technical FAQs

Ask a Question

Is there a part number for the mounting clips for the Magelis HMIGTOxxx0 target?

Yes, the part number for the mounting clips for the HMIGTOxxx0 is HMIZGFIX.


Legacy KB System (APS) Data: RESL213377 V1.0, Originally authored by GeMc on 02/01/2014, Last Edited by GeMc on 02/01/2014
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?