Technical FAQs

Ask a Question

What is the function of the PRWX instruction in Proworx NXT or 32 ?

The function of the instruction is to enable the ability to perform multiple undo / redo commands while online. See details below from the Proworx Programming User Guide and attached pages.

PRWX_info.pdf


Legacy KB System (APS) Data: RESL213333 V1.0, Originally authored by DaSo on 01/29/2014, Last Edited by DaSo on 01/29/2014
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?