Technical FAQs

Ask a Question

Is there a System Word for Scantime in Unity Pro?

Yes. %SW30 contains the current Scantime of the Master Task. There are also other Scantime system words available, please see the attached document.
%SW30-47.pdf


Legacy KB System (APS) Data: RESL213393 V1.0, Originally authored by GeMc on 02/04/2014, Last Edited by GeMc on 02/04/2014
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?