Technical FAQs

Ask a Question

How can I disable the Schneider Electric logo on the boot up of the Magelis?

You can disable the Schneider Electric splash screen in the Vijeo Designer setting of the application. The option is called "Custom Welcome Screen"
under the Options of the Target. You need to uncheck the box and re-download the application into the Magelis screen.


Legacy KB System (APS) Data: RESL213353 V1.0, Originally authored by GeMc on 01/31/2014, Last Edited by GeMc on 01/31/2014
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?