Technical FAQs

Ask a Question

Is the Magelis HMISCUxxx serial port non-isolated?

Yes, the Magelis HMISCU serial port is non-isolated. Non-isolated means that the SG (signal ground) are connected to the FG (frame ground).


Legacy KB System (APS) Data: RESL213379 V1.0, Originally authored by GeMc on 02/01/2014, Last Edited by GeMc on 02/01/2014
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?