Technical FAQs

Ask a Question

Do I need a CHS instruction programmed in Segment one, Network one, of my ProWORX 32 v2.1 project in order for my Quantum Hot Standby configuration to function properly?

No. With ProWORX 32 v2.1, you can use 'Configuration Extensions' in Lieu of the CHS instruction.
You will still be required to install the CHS loadable so that Hot Standby is configurable from 'Configuration Extensions'.




You will also need to define a configuration extension size in the controller properties. The Quantum Hot Standby extension uses 18 words.






Legacy KB System (APS) Data: RESL213342 V1.0, Originally authored by DiSa on 01/29/2014, Last Edited by DiSa on 01/29/2014
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?