Technical FAQs

Ask a Question

Where is the family.DSC file located for installation of the TCPOpen Library for Unity Pro?

TCPOpen Library install for Unity Pro.
Run setup.exe from the TCPOpen installation CD.

The path to the family.dsc file requested by the <Install Family> button depends on the Windows OS:

Windows XP

C:\Documents and Settings\All Users\ApplicationData\Schneider Electric\Unity Pro\custom Libset\V7.0\TCPOPEN\FFBinstall\Advanced


Windows 7:

C:\Program Data\Schneider Electric\Unity Pro\Custom Libset\V7.0\TCPOpenInstall\FFBinstall\Advanced


Note:
During the install you may run into a The LibPath key was not found in registry error.

To correct this, Run Updateforcompanions.bat from the folder on the Unity PRo Installation CD.
"UpdateForCompanions" followed by the letter corresponding to the installed Unity Pro package: "S", "M", "L", "XL"
- For example, D:\updateforcompanions XL.bat


Legacy KB System (APS) Data: RESL213378 V1.0, Originally authored by DaSo on 02/01/2014, Last Edited by DaSo on 02/01/2014
Related ranges: Unitelway
Was this helpful?
What can we do to improve the information ?