Technical FAQs

Ask a Question

Why am I getting the message: "Please contact your local Schneider Representative to convert your Project" when I try to open a Vijeo Designer project?

This means that you are trying to open a project that is not supported with the version of Vijeo Designer you have. For US customers, it is recommended
that you send the project to Customer.Services@schneider-electric.com with your contact information for request to convert application. Non-US
customers, please contact your local Schneider Representative.

The project file should be in *.VDZ or *.swxcf format. We will convert the application with a intermediate version that will support your version of Vijeo
Designer and email that back to you.


Legacy KB System (APS) Data: RESL213382 V1.0, Originally authored by GeMc on 02/01/2014, Last Edited by GeMc on 02/01/2014
Related ranges: Vijeo Designer
Was this helpful?
What can we do to improve the information ?