Technical FAQs

Ask a Question

In Unity Pro, what would cause a datatype not compatible error when adding an ARRAY[1..43] OF INT variable to the 'PID_INT' PARA pin?

If you had already created a variable by double clicking on the pin, it may have created a variable of ARRAY [1..2] OF INT type. This is what is created by default. Since the PARA pin is of the ANY ARRAY variety, it inherits the properties of the first variable assigned. One this occurs, you must delete the PID_INT block entirely and insert a new one, then assign the ARRAY[1..43] OF INT variable.


Legacy KB System (APS) Data: RESL213388 V1.0, Originally authored by DiSa on 02/03/2014, Last Edited by DiSa on 02/03/2014
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?