Technical FAQs

Ask a Question

Is there a way to start an M340 without using Unity Pro or Unity Loader?

Yes. Before loading the project to the M340, an input can be designated for stopping and starting the PLC. You can also configure the M340 to auto start in Run so that anytime that it loads off of the SD card it will go into Run.


Legacy KB System (APS) Data: RESL213376 V1.0, Originally authored by GeMc on 02/01/2014, Last Edited by GeMc on 02/01/2014
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?