Technical FAQs

Ask a Question

PowerPact H- J- and L-Frame and Compact NSX Modbus Communication User Guide

Issue
PowerPact H- J- and L-Frame and Compact NSX Circuit Breakers use different communication parameter and device then other Micrologic circuit like the Masterpact and larger frame size Powerpact and Compact Circuit Breakers. See FA211477 for information on the other breakers.

Product Line

Micrologic Trip Trip Function Breaker Types Type
2.2 (AB, G,M) LSI Compact NSX (250 A) Standard (IEC) (No Comms)
2.3 LSI Compact NSX (630 A)
3.2 LI Powerpact H & J Frame, Compact NSX (250 A) Standard (No Comms)
3.2S LSI
3.3 LI Powerpact L Frame, Compact NSX (630 A)
3.3S LSI
5.2A LSI Powerpact H & J Frame, Compact NSX (250 A) Ammeter
6.2A LSIG
5.3A LSI Powerpact L Frame, Compact NSX (630 A)
6.3A LSIG
5.2E LSI Powerpact H & J Frame, Compact NSX (250A) Energy
6.2E LSIG
5.3E LSI Powerpact L Frame, Compact NSX (630 A)
6.3E LSIG


Environment
Communication applications using Micrologic trip units and circuit breakers with frame sizes less than 630 A.

Cause
Need register lists and a communication guide for Micrologic trip unit.

Resolution
Below are the links to the Modbus user guides.

PowerPact H-, J-, and L- Frame Circuit Breakers Modbus Communication Guide 0611IB1302
Compact NSX 100-630 A Modbus Communication Guide DOCA0091EN

Attached is the legacy user guides

 
Was this helpful?
What can we do to improve the information ?