Technical FAQs

Ask a Question

Can I wire the 2 wires of a self powered actuator to the 170AAO92100 module and not use the modules loop power?

No. The module requires 24V at Pins 17 (-)and 18 (+) of row three for the circuitry to work. If you are forced to use a self powered device with only two wires accessible, you will need to use an external loop isolator.


Legacy KB System (APS) Data: RESL213340 V1.0, Originally authored by DaSo on 01/29/2014, Last Edited by DaSo on 01/29/2014
Related ranges: Modicon Momentum I/O
Was this helpful?
What can we do to improve the information ?