Technical FAQs

Ask a Question

What are the suggested product migration from XBTGT to HMIGTO targets?

Below is the Migration table to go from XBTGT to HMIGTO targets.

*Note : As a reminder, the highlighted XBTGT references will be obsolete at the end of June 2013. Migration to the GTO
for these references should be done as soon as possible. The other XBTGT part numbers will remain active for a number
of years. Migration can be done at your convenience.


Legacy KB System (APS) Data: RESL213373 V1.0, Originally authored by GeMc on 02/01/2014, Last Edited by GeMc on 02/01/2014
Related ranges: Magelis XBT GT
Was this helpful?
What can we do to improve the information ?