Technical FAQs

Ask a Question

How to disable the disclaimer notice for MiCOM S1 Studio

The disclaimer notice will pop up every time that MiCOM S1 Studio is initialized. To disable this disclaimer notice: open MiCOM S1 Studio >click Options > click Preferences > Uncheck the "Show disclaimer notice at start-up" box.


Legacy KB System (APS) Data: RESL213336 V1.0, Originally authored by DaFr on 01/29/2014, Last Edited by DaFr on 01/29/2014
Related ranges: Others protection relays
Was this helpful?
What can we do to improve the information ?